Insert, delete and rename data and tag sets

To insert new data and tag sets, delete existing data and tag sets, or rename data and tag sets, use the
Recipe
menu. When the
RecipePlus
editor is open, the
Recipe
menu becomes available on the menu bar.
The
Recipe
menu contains the following items:
  • Insert Data Set
    Select this menu item to open a dialog where you can specify the name of a new data set. Data set names can have a maximum of 31 characters.
  • Delete Data Set
    Select this item to open a list of the data sets in the recipe. You can then select one or more data sets to delete.
  • Rename Data Set
    Select this item to open a dialog with a list of data sets and a text box for a new data set name. Data set names can have a maximum of 31 characters.
  • Insert Tag Set
    Select this menu item to open a dialog where you can specify the name of a new tag set. Tag set names can have a maximum of 31 characters.
  • Delete Tag Set
    Select this item to open a list of the tag sets in the recipe. You can then select one or more tag sets to delete.
  • Rename Tag Set
    Select this item to open a dialog with a list of tag sets and a text box for a new tag set name. Tag set names can have a maximum of 31 characters.
  • Compare Recipes
    Select this item to open the Compare Recipes dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal