Print graphic displays

To print a graphic display
  1. Choose
    Print
    from the
    File
    menu.
  2. Specify print options such as number of copies.
  3. Click
    OK
    .
    TIP:
    To change the printer or printer options, from the
    File
    menu, choose
    Print Setup
    .
    To print graphic displays at runtime, create a display print button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal