Organize graphic displays in folders

Use folders to organize graphic displays in
FactoryTalk View Studio
. These folders are logical folders and do not represent the actual location of files on your hard drive. They are intended for design time and do not affect the display names at runtime or runtime display navigation. You can create up to two levels of folders.
To organize graphic displays in folders
  1. In the FactoryTalk View Explorer window, expand the HMI server and the
    Graphics
    folder, right-click
    Displays
    , and then select
    New Folder
    .
  2. In the
    Save
    dialog box, enter a name for the folder, and then click
    OK
    .
  3. Create displays in the folder or drag displays to the folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal