Configure a model
Data logging saves specific tag values or data under certain conditions. In the
Data Log Model
editor, you create data log models that define these conditions. The data can be shown in a trend.When you configure a model you specify how many log values to store, where log files will be stored, the conditions that will trigger data logging, and which tags the model will monitor.
You can define multiple data log models, but at runtime you can use only one data log model at a time.
TIP:
For data logging to occur at runtime, you must select the
Data logging
box in the Startup
editor.The maximum number of tags that can be logged is 100 tags.
To configure a model
- Open theData Log Modeleditor using one of these methods:
- In theData Logfolder in theExplorerwindow, double click theData Log Modelicon.
- In theData Logfolder in theExplorerwindow, right click theData Log Modelicon and selectNew.
- In theData Logfolder in theExplorerwindow, drag and drop theData Log Modelsicon into the right pane.
- In theData Logfolder in theExplorerwindow, right-click an existing data log model and selectOpen.
- From theFilemenu, selectNew > Data Log.
- Define the model on theSetup,Paths,Log Triggers, andTags In Modeltabs.
When you click
Close
to save the model, type a name for it in the Component Name
dialog box.Provide Feedback