Information displayed in the web client Logs view
Select the
in the view menu to display logged events from the server.
Logs
icon
in the view menu to display logged events from the server.
TIP:
To prevent log files from growing too large,
FactoryTalk
Updater saves events for four months and then discards them.This table describes the columns of information listed in the Logs view.
Column | Description |
|---|---|
Provider | The source of the logged message or event. |
Time | The time and date the event occurred. |
Message | A description of the event, including recommended or required action. |
Provide Feedback