Information displayed in the web client License Information tab

The
License Information
tab in the
Activations
view lists license information for all machines or for machines in a group. Enter a search term in the
Search
box to filter the list based on that term.
This table describes the columns on the
License Information
tab.
Column
Description
Product
The
Rockwell Automation
software application.
Serial #
The serial number of the product.
Expires
The expiration time and date for the activation.
Activation
The name of the activation.
Feature Version
The feature version of the license.
Location
The machine name of the activation server.
Tip:
The
Location
box displays only the first 15 characters in the activation server name. Names longer than 15 characters are truncated.
Total
The number of activations purchased with the product.
In Use
The number of activations used for each product. Select the number in this column to see more details, such as the computer that checked out or borrowed the activation, the number of activations checked out or borrowed, and whether the activation is concurrent or borrowed. No details are available if the number in this column is zero.
Borrowed
The number of activations borrowed from an activation server. Select the number in this column to see more details, such as the computer that borrowed the activation, the date the activation was borrowed, and the date the borrowed activation expires. No details are available if the number in this column is zero.
Product Version
The product version activated. Some activations are for multiple product versions. This field displays
n/a
if not used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal