Information displayed in the Transactions tab

The
Transactions
tab in the
Activations
view displays a log of license events, or transactions, for all machines or for machines in a group.
TIP: To prevent transaction log files from growing too large,
FactoryTalk
Updater saves transactions for four months and then discards them.
This table describes the columns on the
Transactions
tab.
Column
Description
Time
The date and time the transaction occurred.
Activity
The type of transaction, for example, a license return, borrow, check out, rehost, or get.
Machine Name
The name of the machine that carried out the transaction.
User Name
The user who conducted the transaction.
Feature Name
The executable file for the licensed
Rockwell Automation
software application, for example, RS5000.exe.
Product
The name of the licensed
Rockwell Automation
software application.
Serial Number
The serial number of the licensed
Rockwell Automation
software application.
Quantity
The number of licenses included in the transaction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal