Switch or add servers
Switch to another Updater server to view and manage machines on that server or add a server
to the server list.
When switching or adding a server, the
FactoryTalk
Updater server verifies
the credentials of the client machines. The server requests credentials when the client and
server are on different machines. The server does not request credentials when the client
and server are on the same machine.To switch or add servers
- On the main menu bar, selectSwitch Server.
- Select a server from the list to switch to that server. When requested, enter theUser NameandPasswordcredentials for theWindows®account of the Server machine.
- To add a server to the list, select theaddicon
to open the Add New Serverdialog box. - Enter the name or IP address of the server to add. When requested, enter theUser NameandPasswordcredentials for theWindows®account of the Server machine.
- SelectOK. Updater automatically switches to the new server.
Provide Feedback