Information displayed in the TRANSACTIONS tab
The
TRANSACTIONS
tab in the Activations
view displays a log of license
events, or transactions, for all machines or machines in a group.
TIP:
To prevent transaction log files from growing too large,
FactoryTalk
Updater saves transactions for four months and then discards
them.This table describes the columns on the
TRANSACTIONS
tab. Column | Description |
|---|---|
Time | The date and time the transaction occurred. |
Activity | The type of transaction; for example, a license return, borrow, check out, rehost, or get. |
Machine Name | The name of the machine that carried out the transaction. |
User Name | The user who conducted the transaction. |
Feature Name | The executable file for the licensed Rockwell Automation software application; for example, RS5000.exe. |
Product | The name of the licensed Rockwell Automation software application. |
Serial Number | The serial number of the licensed Rockwell Automation software application. |
Quantity | The number of licenses included in the transaction. |
Provide Feedback