Export the OT Mode software list to a Zip file
When you are working in an OT environment, use OT Mode to manage Rockwell Automation
software on the agent. Since an OT environment is disconnected from the Internet, OT Mode is
dependent on the IT Mode to obtain the latest information and patches.
From OT Mode, export the software list to a server or USB drive. From either location, paste
the software list to the IT environment.
- From the menu, select .
- In theSave towindow, selectBrowse.
- In theSave Aswindow, enter the name of the exported file, and selectSave.
- Enter a password for the file.
- Confirm the password and selectOK.
- Copy the exported.zipfile to the IT environment file server.
Provide Feedback