Configure a destination for file downloads
Select a destination for saving files downloaded by
FactoryTalk
Updater.To configure a destination for file downloads
- On the main menu bar, selectDownload Locationto open theSet Download Locationdialog box.
- Enter the destination for downloads or click the browse icon
to browse to a destination and select it.The default destination is C:\Users\<username>\Downloads.
Provide Feedback