FactoryTalk Updater command-line parameters
This table identifies the command-line parameters used to export inventory and configure
FactoryTalk
Updater Client and Server. Command-line parameters are
case-insensitive. However, if a specified value includes a space, be sure to enclose the
value in quotation marks (for example, "value with spaces").Parameter | Description |
|---|---|
/? | Displays the usage options for parameters. |
/ExportInventory="value" | Exports the inventory information from all online Agents. Specify the value of an existing directory path or the full path for the file to export. The file to export must be a .csv file. |
/ExportActivation="value" | Exports activation information from all online Agents. Specify the value of an existing directory path or the full path for the file to export. The file to export must be a .csv file. |
/ExportLog="value" | Exports the log information from the Client. Specify the value of an existing directory path or the full path for the file to export. The file to export must be a .csv file. |
/ExportAop="value" | Export Add-On Profile (AOP) information from all online agents to local. You can
specify the value of an existing directory path or the full path for the file to
export. The file to export must be a .csv file. If the value is a directory, it
must exist. |
/ExportCompatibility="value" | Export product compatibility issues from all online agents to a comma-separated
value (CSV) file. |
/DownloadPath="value" | Specifies the download path of the Client. The value of this parameter must be an existing directory path. |
/CheckInterval="value" | Specifies the interval schedule for the automatic scanning of all machines. Set this parameter to a value between 1 and 366 days. |
/AddAgents | Adds agents to the server by a single IP address or by a range of addresses.
Specify agents in this format: /AddAgents="10.108.1.1,10.224.1.1-10.224.1.100" |
/Group | Specifies a group name when adding agents to the server. |
/UserName | Specifies the username used to connect to the Server. |
/Password | Specifies the password used to connect to the Server. |
Example
This example shows how to use the command-line parameters to export information:
CommandPrompt.exe /ExportInventory="C:\InventoryInfo\InventoryInfo.csv" /ExportActivation="C:\ActivationInfo\Activations.csv" /ExportLog="C:\ClientLog\Log.csv" /ExportAop="C:\AopInfo\Aop.csv" /ExportCompatibility="C:\CompatibilityIssuesFolder\CompatibilityIssues.csv" /UserName="user" /Password="password"
This example shows how to use the command-line parameters to add agents and specify a group name:
CommandPrompt.exe /AddAgents="10.108.1.1,10.224.1.1-10.224.1.100" /Group="groupA" /UserName="user" /Password="password"
Provide Feedback