Download and deploy patches
Use the
Machines
view to download the latest patch available for installed Rockwell Automation
software. Before downloading patches, log into the Rockwell Automation
Product Compatibility and Download Center (PCDC), and log onto the server as an administrator.- To log into PCDC and to the server:
- On the main menu bar, selectAccountto open theAccountdialog box.
- UnderPCDC Login, selectGo to login pageto open a browser window to the PCDC login page. Enter your credentials.
- SelectServer Loginand enter your credentials for logging into the server as an administrator.
- From theMachinesview, select the applications to update.TIP:To view information for a patch, select the information icon to open the release notes from the PCDC.
- SelectDownload and Deploy. TheDownload and Deploydialog box lists the machines to be updated. SelectMore detailsto see a list of the patches that will be deployed.
- Select the time for installing patches and restarting the patched machines:
- SelectImmediatelyto install patches or restart machines when you selectDeploy.
- SelectSpecific timeto enter a date and time for the installation and restart.
- To use the time zone configured on the Updater client machine, selectTime zone based on the client's local time. By default, the check box is not selected, and Updater uses the time zone configured on the agent machines to be patched.
- SelectDeploy. TheLatest Patchcolumn on theMachinespage displays the patch progress.
- When the download and deploy is complete, selectResultsfor a summary of the operation.
Provide Feedback