FactoryTalk Optix Studio Pro upgrade overview

To use FactoryTalk Optix Studio Pro, follow the steps below.
  1. Activate a FactoryTalk Optix Studio Pro entitlement  for a user. That user can then use FactoryTalk Optix Studio Pro on an online computer, an offline computer, or in a different organization.
    TIP:
    A FactoryTalk Optix Studio Pro entitlement is associated to a specific user, who can be a member of multiple oganizations.
    A user can keep on using their Pro entitlement as they toggle from one organization to another. In this way, they do not need a separate entitlement for each organization they belong to.
  2. IMPORTANT:
    Runtime Tools are already embedded in OptixPanels™ and EEC (Embedded Edge Computes).
    You have to download, install and activate Runtime Tools for Windows and Linux devices.
NOTE:
You can rehost both a FactoryTalk Optix Studio Pro entitlement and a Runtime Tools entitlement.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.