Optix Runtime with Base Token Package (S)

The following example shows a system architecture that uses a panel PC and two controllers.
System Architecture - Base Package S
A diagram of sample S system.
The example architecture has the following components.
  • Single HMI runtime with a touch screen and typical HMI functionality
  • Communicates with a
    Rockwell Automation®
    controller and a third-party controller
  • Logs data to an internal database
  • Requires event logging, alarming, and recipe
The following table shows example runtime sizing for a package that includes the application components.
Selection
Base Token Value
Extended Token Value
Clients
Native HMI client
1
-
Features
Alarms
1
-
Recipe
1
-
Runtime retentivity
1
-
Event logger
1
-
Data logger
1
-
Embedded database
0
-
Controller Connections
Rockwell Automation®
EtherNet/IP™
- 1 connection
1
-
Third-party drivers - 1 connection
1
-
Total:
8
0
Base token package (S), which includes eight base tokens, is recommended for this example. There is no need for an extended package. Use the Device Sizing tool to select the best deployment option for your application.
For this configuration, you can select one of the following deployment options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal