Call Home entitlement mechanism
The Call Home entitlement mechanism consists of an entitlement scheme available for
FactoryTalk®
Optix™
Runtime running in Docker containers only.FactoryTalk®
Optix™
Runtime can be run in Ubuntu 22.04 Docker containers.The entitlement serial number is injected into the Docker container as an environment
variable named
FTOPTIX_ENTITLEMENT_SERIAL_NUMBER
. This variable triggers the
Call Home mechanism.The entitlement flow occurs as follows:
- The Docker container calls specific Entitlement Web APIs to lock the specified entitlement.
- If the lock request is successful, the Docker container periodically refreshes the entitlement lock every 30 minutes.
- The Docker container unlocks the entitlement upon Runtime termination, to make it available for rehosting.
TIP:
If the Docker container does not unlock the entitlement upon termination,
proceed with a manual rehost. This scenario might occur
whenever Runtime stops unexpectedly.
If the Docker container rehosts the locked entitlement during runtime, this latter receives a
rehost notification after the next entitlement lock refresh.
A seven-day grace period starts only if the connection with the Entitlement Web API is lost
after an entitlement lock.
Provide Feedback