Find broken dynamic links
You can display all incorrect dynamic links from a project in the
Output Pane
.- Unresolved links
- Broken links
- Invalid links
- Broken pointers
- In the main toolbar, selectFind dynamic links.
Broken links display in the
Output Pane
. Each result provides a path
to the parent object, link value and result kind. You can use the filter buttons to include
and exclude specific broken link types from search results.Broken links display
in
the property while unresolved links display
.
in
the property while unresolved links display
.You can click the displayed path to navigate to the broken link.
Provide Feedback