Import controller variables

Configure a communication driver to import sample tags (controller variables) from a Logix controller.
TIP: Instead of importing controller variables from a Logix controller, you can create variables manually. See Create variables.
Prerequisites
In the Logix Designer application, download the LogixTags.ACD project to a physical Logix controller or an emulated
FactoryTalk® Logix Echo™
controller. Set the controller in the run mode.
For more information, see the Logix Designer online help.
  1. To import controller variables
  2. From the toolbar, select
    Open dashboard page
    .
  3. In the editor, select
    Configure communications to devices
    .
  4. Select
    New stations
    .
  5. Select
    RA EtherNet/IP Station
    and select
    Next
    .
  6. (optional) To import the controller tags in the online mode, in
    Route
    , enter
    IP_Address
    \Backplane\
    Chassis_Slot_Number
    and select
    Next
    .
    TIP: For more information, see RA EtherNet/IP Driver.
  7. Select
    Next
    .
  8. Fetch the controller tags:
    • To fetch the controller tags in the offline mode, select
      Browse
      and select the downloaded
      LogixTags.ACD
      file.
    • To fetch the controller tags in the online mode, select the
      Offline/Online
      toggle to change it to the
      Online
      position.
  9. Select all controller tags and select
    Next
    .
    Selected tags in the online mode
  10. Select
    Exit
    .
In
Project view
, the imported controller variables are available in the
ProjectName
CommDrivers
RAEtherNet/IPDriver1
RAEtherNet/IPStation1
Tags
Controller Tags
node. Note this location.
Imported controller variables
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal