Create Alarm manager and Alarm summary

Create an
alarm manager
and
alarm summary
widgets, to display essential information about alarms in the project.
  1. In the main toolbar, select
    Template Libraries
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Widgets
    .
  3. Under
    Components
    , drag
    Alarm Widgets
    to a folder in the
    UI
    folder.
    AlarmSummary# (type)
    and
    AlarmManager# (type)
    appear in the folder.
  4. In
    Template Libraries
    , select
    Close
    .
  5. (optional) On the editor, configure the properties of the two widgets.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal