Alarm Details view

You can open view from
Alarm Summary
  or
Alarm Manager
to display detailed information about a selected alarm.
Alarm details
Alarm variable
Description
Current state
Current state for Alarm Summary. The Current state field displays value depending on the alarm logic.
Message
Message associated with the alarm event, which displays when the alarm is active. Displays the message for the highest alarm state applicable.
Status
Status displays a combination of all the conditions of an alarm. If any condition in the alarm is In Alarm or Unacknowledged, the alarm appears as In Alarm or Unacknowledged.
Severity
The numeric value mapped to the assigned priority of the alarm condition.

    1-250 (Low)

    251-500 (Medium)

    501-750 (High)

    751-1000 (Urgent)

Confirmed
Displays if the alarm is confirmed.
Unconfirmed
Displays if the alarm is unconfirmed.
Inhibit state
When an alarm has more than one inhibit state, the icon of the highest inhibit state appears in the table. If no icon appears, the alarm has good quality, and is not disabled, suppressed, or shelved.
Name
Name of the alarm object that generated the alarm event.
Source variable
Variable monitored by the event.
Quality
Displays information of a fault in case of faulted alarms.

    Good - alarm is not in faulted state

    Bad - alarm is in faulted state: controller cannot be reached or InFaulted variable for IBA/TBA is set to true.

Event time
The date and time the alarm event occurred.
In alarm time
The time the selected alarm entered the In Alarm state.
Out of alarm time
The time the selected alarm entered the Normal or Out of Alarm state
Shelve duration
The default time for which the selected alarm condition is shelved to prevent the notification of new state changes. Shelve duration is assigned to the alarm in the project
Max Time Shelved
The maximum time the alarm can be shelved.
Shelve Time
The time the selected alarm was shelved.
Unshelve Time
The time the selected alarm was unshelved. If the alarm is currently shelved, this is the time the alarm is unshelved automatically when the shelve duration expires.
Enable time
The time the selected alarm was enabled
Disable time
The time the selected alarm was disabled.
Suppress time
The time the selected alarm was suppressed
Unsuppress time
The time the selected alarm was unsuppressed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal