Edit a recipe schema

You can edit recipe schema properties by using a dedicated interface built into
FactoryTalk Optix
.
  1. To edit a recipe schema
  2. From the toolbar, select
    Open dashboard page
    .
  3. In the editor, select
    Configure a recipe
    .
  4. Select the recipe that you want to edit.
  5. If needed, edit the
    Name
    and
    Target node
    properties.
  6. Select
    Next
    .
  7. Select an existing database or configure a new database:
    • To use an existing database:
      1. Select an existing database.
      2. If necessary, edit the database properties.
      3. Select
        Next
        .
    • To create a database:
      1. Select
        New database
        .
      2. If needed, edit the
        Name
        and
        Type
        fields.
      3. Select
        Next
        .
      4. If necessary, edit the database properties.
      5. Select
        Next
        .
    • To duplicate an available database:
      TIP: Duplicating an existing database allows you to create a database base on the existing database quickly.
      1. Right-click an available database and select
        Duplicate
        .
      2. If necessary, edit the database properties.
  8. Select
    Next
    .
  9. Select the recipe parameters to use.
    TIP: You can show or hide variables (parameters) nested in other variables by using the
    Nested variables
    toggle. You can quickly find the parameters that you want to select by using the
    Search
    field.
  10. Select
    Next
    .
  11. Review the settings.
  12. Select
    Exit
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal