Add an OPC UA server
Configure an OPC UA server by adding the OPC UA server object to the project and by editing the properties of the server.
- InProject view, right-clickOPC-UAand select .
- InProperties, configure the OPC UA server.
- Endpoint URL. The communication protocol and network address of the endpoint on the OPC UA server.
- Maximum number of connections. Maximum number of OPC UA clients that can connect to the OPC UA server.
- Use node path in NodeIds. Publish nodes with IDs that display the node path in this formatns=. For example,<namespace>;s=Path.To.Nodens=7;s=NewHMIProject1.Model.AnalogVariable1.
- Sampling interval. Time interval between successive readings of the field variables by the OPC UA server.
- Max array length. The maximum number of elements in an array.
- Minimum message security mode:
- None. The messages may be unsigned and unencrypted.
- Signature. The messages must be signed or signed and encrypted.
- Signature and encryption. The messages must be signed and encrypted.
- Minimum security policy:
- None. The OPC UA server does not require any specific security policy.
- Basic256Sha256. The OPC UA server requires this security policy or a more secure policy.
- Aes128_Sha256_RsaOaep. The OPC UA server requires this security policy or a more secure policy.
- Aes256_Sha256_RsaPss. The OPC UA server requires this security policy.
- Server certificate file. The publicDERcertificate file of the OPC UA server (X509v3).TIP:The server certificate file must be in theFTOptixApplication/ProjectFiles/PKI/Own/Certsfolder.If specified, the private key must also be specified. If not server specified, it is automatically generated at runtime in theFTOptixApplication/ApplicationFiles/PKI/Own/Certsfolder.
- Server private key file. The privatePEMkey file of the OPC UA server encoded with ASCII Base64.TIP:The server private key file must be in theFTOptixApplication/ProjectFiles/PKI/Own/Certsfolder.If specified, the certificate must also be specified. If not specified, it is automatically generated at runtime in theFTOptixApplication/ApplicationFiles/PKI/Own/Certsfolder.
- Product URI. A URI that globally identifies the software.
- Product name. The name of the software.
- Manufacturer name. The name of the software manufacturer.
- InProperties, next toNodes to publish, select.
A configuration of nodes to be published appears underNodes to publish.IMPORTANT: Every Publishing nodes always publishes child nodes. - InConfiguration:#
- Add a node. Next toNodes, selectand configure the node by editing its properties. Repeat if necessary.

- Add a user Next toUsers, selectand configure the user. Repeat if necessary.
IMPORTANT: If you expose specific nodes instead of the entire project, you must specify at least one user. The user can be the default Anonymous user. - To expose business logic nodes to OPC UA clients setPublishDynamicConfigurationNodestoTrue.Business logic nodes include dynamic links or linked variables, converters, and event handlers or methods associated to events.
opc ua server
Provide Feedback