Micro Controller Driver
Observe these guidelines when working with Micro Controller Driver.
Supported controllers
Micro Controller Driver supports
Micro800™
controllers and MicroLogix™
1400 controllers, as well as SLC 500 controllers.
TIP:
If you use a 1761-NET-ENI(W) module to communicate to the serial port of a supported controller, you must use a Series C or Series D 1761-NET-ENI(W) module to work with FactoryTalk Optix.
Controller tags import
With Micro Controller Driver, you can import tags from
Micro800
controllers in the online mode.
This communication driver supports importing custom data types defined in the controller project.
Data types
Micro Controller Driver supports these data types:
Datatype | FactoryTalk Optix datatype |
|---|---|
BOOL | Boolean |
SINT | SByte |
DINT | Int32 |
REAL | Float |
STRING | String |
LREAL | Double |
INT | Int16 |
LINT | Int64 |
USINT | Byte |
BYTE | |
UINT | UInt16 |
WORD | |
UDINT | UInt32 |
DATE | |
TIME | |
DWORD | |
ULINT | UInt64 |
LWORD |
micro controller
micro controller driver
Provide Feedback