Alarm types
Different alarm types become active under different circumstances.
Alarms types and when they activate include:
Alarm type | Description | Example |
---|---|---|
| Activates when the Boolean value of the monitored variable is not the normal value. | Monitor a variable for the open or closed status of a firewall. An alarm event occurs if the closed normal condition is not met. |
| Activates when the value of the monitored variable reaches one or more limits of interest. | Monitor temperature. If the low limit is 10 °C and the high limit is 100 °C, an alarm event occurs when the temperature reaches either limit. |
| Activates when the value of the monitored variable reaches an offset equal to or greater than the set variable. | Monitor a temperature that must be kept constant. If a setpoint value is set to 50 °C, and the temperature drop limit is -3°, and temperature increase limit is +3°, an alarm event occurs when the temperature reaches either 47 °C or 53 °C. |
| Activates when the change rate of the value of the monitored variable reaches one or more set limits. | Monitor the value of a variable that represents the speed of a conveyor belt. The variable will be polled every five seconds and the change limit is set to 10. If the measurement shows that the rate of change of the conveyor belt speed is greater than or equal to 10 when compared to the previous sample value, an alarm event occurs. |
| Signals all corresponding levels up to four levels when several limits of interest are reached consecutively. Levels include low-low, low, high, and high-high. | If a temperature that starts from a normal value reaches the high-high level, an alarm event signals both the high-high and high level. |
| Signals only the last of up to four levels reached when several limits of interest are reached consecutively. | If a temperature that starts from a normal value reaches the high-high level, the alarm signals only the high-high level. |
TIP:
Both exclusive and non-exclusive alarms monitor the same types of values. But when several limits of interest are reached consecutively:
- An exclusive alarm signals only the last limit reached.
- A non-exclusive alarm signals all the limits reached
The analog alarm grid displays the last limit reached on the exclusive alarm and all the limits reached by the non-exclusive alarm. In the alarm grid, alarm history grid, and alarm banner, exclusive alarms display the same information as non-exclusive alarms.
For example, if variable values monitored by an exclusive and a non-exclusive alarm reach their High limit and High-High limit:
- Alarm banner shows the latest alarm for both
- Alarm grid shows High-High alarm for both
- Analog alarm grid:
- shows High-High on the current state for the exclusive alarm, which is the last limit reached
- shows four columns (Low-Low, Low, High, High-High) where High and High-High are marked as active for the non-exclusive alarm
- Alarm history grid shows a record for every limit that has been reached on each alarm for both.
Logix alarms
Logix alarms are imported at runtime if you enable
Use Alarms
on the controller. The importcreates equivalent Optix alarm objects, listed in the following table:Logix alarm type | Optix alarm type (after import) |
---|---|
|
|
| Up to two alarms:?
|
| Depending on the condition:
|
To enable backing tags, you must enable
Extended Properties
on your controller. See Extended properties. Alarm backing tags provide additional information about a specific tag-based alarm. Alarm backing tags are located in the @Alarms
subfolder of a specific tag. Alarm Backing Tags

alarm
digital
exclusive deviation
exclusive level
exclusive limit
exclusive rate of change
non-exclusive deviation
non-exclusive level
non-exclusive limit
non-exclusive rate of change
Provide Feedback