Create an Advanced SVG Image
    Prerequisites
Download the star_rectangle.svg image.
- To create an Advanced SVG Image
- InProject view, right-clickMainWindow (type)and select .
- Double-clickMainWindow (type).
- Double-click the empty imageon the canvas.
- Select. Import file(s) Import file(s)
- InImport file(s), select the file to import and then chooseSelect.
Provide Feedback