Create elements for controlling the current value
    Create a gauge and other interface elements that display the current value and enable you to edit it.
- Create the current value label:- InProject view, right-clickMainWIndow (Type)and select .
- Hover-over a gauge, select, and enter CurrentValueLabel. CurrentValueLabel.
- InPropertiesand setTexttoCurrent Value.
 
- Create the value gauge:- Right-clickMainWindow (Type)and select .
- Hover-over a gauge, select, and enter ValueGauge. ValueGauge.
- InProperties, create a dynamic link between theValueand .For more information about dynamic links, see Create dynamic links.
 
- Set the value gauge warning zone 1:- InProperties, next toWarning zones, select. 
- UnderWarningZone1, setColorto#f30000.
- Create a dynamic link betweenFromand .For more information about dynamic links, see Create dynamic links.
- Create a dynamic link betweenToand .For more information about dynamic links, see Create dynamic links.
 
- Set the value gauge warning zone 2:- Next toWarning zones, select. 
- UnderWarningZone2, setColorto#02d92d.
- Create a dynamic link betweenFromand .For more information about dynamic links, see Create dynamic links.
- Create a dynamic link betweenToand .For more information about dynamic links, see Create dynamic links.
 
- Set the value gauge warning zone 3:- Next toWarning zones, select. 
- UnderWarningZone3, set theColorproperty value to#f30000.
- Create a dynamic link betweenFromand .For more information about dynamic links, see Create dynamic links.
- Create a dynamic link betweenToand .For more information about dynamic links, see Create dynamic links.
 
- Create the value label:- InProject view, right-clickMainWIndow (Type)and select .
- Hover-over a gauge, select, and enter: ValueLabel. ValueLabel.
- InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
 
- Create the value spin box:- InProject view, right-clickMainWIndow (Type)and select .
- Hover-over a gauge, select, and enter: ValueSpinBox. ValueSpinBox.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
 
- Create the value text box:- InProject view, right-clickMainWIndow (Type)and select .
- Hover-over a gauge, select, and enter: ValueTextBox. ValueTextBox.
- InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
 
Provide Feedback