Create a constrained variable
    Create a variable with high and low value limits that will be linked with the gauges.
- InProject view, right-clickModeland select .
- Hover-over the variable, select, and enter ConstrainedVariable. ConstrainedVariable.
- InProperties, setConstrainedVariable (Int32)to30.
- Right-clickConstrainedVariableand select .
- UnderEURange, set the properties:- SetConstrainttoTrue.
- SetHigh limitto50.
- SetLow limitto20.
 
Provide Feedback