Create a button that closes the application
    Create a button that closes the 
FactoryTalk Optix Application
 application.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enter CloseApplicationButton. CloseApplicationButton.
- InProperties, setTexttoClose application.
- InEvents, next toMouseClick event, selectand select . 
Provide Feedback