Add predefined UI elements 
    Add a login form, a username label, and a clock NetLogic from the template libraries.
- From the toolbar, select.Template Libraries
- Add and configure the login form:- InLibraries, search forLogin Form.
- UnderComponents, dragLogin FormontoMainWindow (type)inProject view.
- InProperties, create a dynamic link betweenUsersand .For more information about dynamic links, see Create dynamic links.
 
- Add and configure the username label:- InLibraries, search forUsername Label.
- UnderComponents, dragUsername LabelontoMainWindow (type)inProject view.
 
- Add the clock NetLogic:- InLibrarieswindow, search forClock.
- UnderComponents, dragClockonto theNetLogicinProject view.
 
- InLibrarieswindow, selectClose.
Provide Feedback