Create a variable
    Create a variable that indicates the current temperature.
- Create the variable:- InProject view, right-clickModeland select .
- Hover-over the variable, select, and enter Temperature. Temperature.
 
- Configure the variable:- InProperties, selectInt32and selectFloat.
- Right-clickTemperatureand select .
- UnderEURange, setHigh limitto100.
 
Provide Feedback