Create a speed gauge and labels
    Create UI elements that display speed-related information about a selected motor.
- Create the speed gauge:- InProject view, right-clickMotorSpeedPaneland select .
- Hover-over the gauge, select, and enter SpeedGauge. SpeedGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
 
- Create the speed label:- InProject view, right-clickMotorSpeedPaneland select .
- Hover-over the label, select, and enter SpeedLabel. SpeedLabel.
- InProperties, setTexttoSpeed.
 
- Create the speed value label:- InProject view, right-clickMotorSpeedPaneland select .
- Hover-over the label, select, and enter SpeedValueLabel. SpeedValueLabel.
- InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
 
Provide Feedback