Create a thermometer linear gauge
    Create a linear gage with a warning zone that indicates the current temperature.
- Create and configure the gauge:- Right-clickMainWindow (Type)and select .
- Hover-over a gauge, select, and enter ThermometerGauge. ThermometerGauge.
- InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
 
- Set the value gauge warning zone:- InProperties, next toWarning zones, select. 
- UnderWarningZone1, setColorto#f30000.
- SetFromto75.
- SetToto100.
 
Provide Feedback