Save and commit changes
    Save your progress and commit changes to the local version-control repository.
- From the toolbar, select. Save and Commit Save and Commit
- If needed, in the prompt, selectOpen FactoryTalk Optix Studio optionsto configure your user name and email.The user name and email are needed to commit changes to the repository.
- Enter a meaningful commit message.For example, enterConfigured quick start project.
- SelectOK.
To see the commits history and restore the project to a commit, select  .
 .
 
 View history
Commits history

Provide Feedback