Variables
    A variable is an element that represents a figure or a characteristic of an object and specifies the value of that characteristic.
Variable overview
      Each variable:
        
- Contains a DataType attribute
- Can be structured to contain other variables
- Contains descriptive attributes
- Cannot contain objects
     TIP: 
    You cannot remove properties from predefined objects. For example, you cannot remove the 
Text
 property from a Label
 object.Variable examples
      For example, a variable can represent:
        
- The speed of a physical object
- TheSpeedvariable with a numeric (Int32) value defines the speed of the Motor object. 
- A style characteristic of a graphic object
- TheText colorvariable defines the color of the Label object 
- Various object properties
- A dynamic link to theEmbeddedDatabase1object defines the Store variable value. 
Provide Feedback