IUAVariable.RemoteRead(timeoutMilliseconds)
    Returns the value of the variable on which it invokes. The optional argument sets the timeout period.
UAValue RemoteRead(doubletimeoutMilliseconds);
Arguments
      - timeoutMilliseconds(double)
- The timeout period, expressed in milliseconds, after which the API throws an exception.TIP: If not specified, the default value of the argument is30000(30 seconds).
Returns
      - UAValue
- The value of the variable.
Example
      In the following example, the 
Speed
 variable value is read and given in an information message.
        var currentSpeed = Project.Current.GetVariable("Model/Motor/Speed"); var value = currentSpeed.RemoteRead(); Log.Info(value.ToString());
Provide Feedback