InformationModel.SetTranslation(localizedText)
    Updates a translation associated with an existing key, based on the argument properties.
void SetTranslation(LocalizedTextlocalizedText);
Arguments
      - localizedText(LocalizedText)
- A C# object with theTextId,Text, andLocaleIdproperties that identify the key and related translation to be updated.
Example
      The following example shows an API that writes the 
New translation
 string for the en-US
 locale associated with the Key1
 key.var localizedText = new LocalizedText("Key1", "New translation", "en-US"); InformationModel.SetTranslation(localizedText);
Provide Feedback