Create objects
    Use C# APIs to create objects in the 
FactoryTalk Optix Studio
 project and return the corresponding C# objects.The APIs are supplied by the 
InformationModel
 class, displayed by the FTOptix.HMIProject
 module.Provide Feedback