Duplicate a client device
    Duplicate a client device to configure another similar client device. 
- From the main toolbar, next to, select the client dropdown menu.Run
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select a client device.
- Select.Duplicate
Configure the duplicated client device properties.
Provide Feedback