Import a FactoryTalk Optix Application
    To deploy an exported 
FactoryTalk Optix Application
, move the file to the client device and run the file.Prerequisites
- To import aFactoryTalk Optix Application
- Move the exported files to the client device.For example, attach the USB drive with the exported application to the client device.
- RunFactoryTalk Optix Applicationon the client system:- OnWindows®client devices, double-clickFTOptixRuntime.exe.
- On Linux client devices, in the terminal, navigate to theFTOptixRuntimefile folder and enter./FTOptixRuntime.
- OnOptixPanel, access the web interface and then selectImportunderLoad application from USB.
 
Provide Feedback