Delete a user
    Delete a user to no longer have the user be a user of the project. 
Delete a user from either the dashboard page or 
Project view
.- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, underUsers, select the users to delete.
- SelectDelete.TIP: You can also right-click the user to delete from eitherManage users and groupsorProject view, and then selectDelete.
The user is removed from the dashboard page and 
Project view
. If the user was assigned to a group, the user no longer appears as a member of the group.Provide Feedback