Change user properties
    Change the properties of a user to modify the domain, password, location, and language for that user.
- InProject view, expandSecurity.
- ExpandUsers.
- Select a user.
- InProperties, change:- Name. Name of the user.
- Password. Password that the user must provide to log on to the application.
- Locale. Location of the user.
- Languages. Language configured for the user.
- Measurement system. The measurement system used to display data to the user:- International system of units
- US customary measurement system
- British imperial units
 
- Domain. Identifies the localWindows®user account for a domain-linked user account.
 
Provide Feedback