Assign a user to a group or role
    Manage users and groups from the dashboard page to assign users to groups and roles in order and create a hierarchy of rights and privileges.
Create users and groups and roles and then assign users to the groups and roles.
- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, either:- UnderUsers, drag a user onto a group underGroupsor onto a role underRoles. You can also drag a group or role onto a user. Hold downShiftorCtrlto select and drag consecutive or multiple selections.
- Select one or more users, selectAssign to groups or roles, select the groups and roles, and then selectApply.
 TIP: appears next to a group or role that is already assigned to a user. You can assign the user to a group or role from Project viewby dragging the user to the group or role inProject view. appears next to a group or role that is already assigned to a user. You can assign the user to a group or role from Project viewby dragging the user to the group or role inProject view.
The user appears under the group on the dashboard page. 
assign
hierarchy
privilege
    
Provide Feedback