Add a user
    Add users to 
Project view
 or Manage user and groups
. Manage existing users by adding users to groups and roles and granting users permissions. - In the main toolbar, selectOpen dashboard page, and then selectManage users and groups.
- UnderUsers, selectAdd user.TIP: To add users inProject view, inProject view, right-click the project node and then select . Right-clickSecurityand select to add a folder for users.
- InAdd Userconfigure the properties for the user:- Name. Name of the user.
- Password. Password that the user must provide to log on to the application.
- Locale. Locale of the user.
- Languages. Language configured for the user.
- Measurement system. The measurement system used to display data to the user:- International system of units
- US customary measurement system
- British imperial units
 
- Domain. Identifies the localWindows®user account for any domain-linked user account.TIP: You can configure the properties for a user fromProject viewby selecting the user and then changing the properties inProperties.
 
- (optional) If groups are created, underAssign groups to user, select the groups to assign to the user.
- (optional) If roles are created, underAssign roles to user, select the roles to assign to the user.
- SelectAdd.UnderUsers, the groups and roles assigned to the user appear. UnderGroups, the user appears under the selected groups. UnderRoles, the user appears under the selected roles.
The user appears under 
Users
 on the dashboard page and in Project view
.user
    
Provide Feedback