Rename a group
    Rename a group to change the name of the group to which users are assigned. You can rename one group at a time.
Rename a group from either the dashboard page or 
Project view
.- Either:- Selectand then selectOpen dashboard pageManage user and groups.
- InProject view, expandSecurityandGroups.
 
- UnderGroups, right-click the group to rename.
- SelectRenameand type a new name for the group.TIP: To rename a group fromProject view, right-click the group, selectRename, and then enter the new name.
The group is renamed on the dashboard page and in 
Project view
. Provide Feedback