Assign a group to a user or role
    Assign groups to users and roles to create a hierarchy of users with assigned rights and privileges.
- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, either:- UnderGroups,drag a group onto a user underUsersor onto a role underRoles. You can also drag a user or role onto a group. Hold downShiftorCtrlto select and drag consecutive or multiple selections.
- Select one or more groups, selectAssignto users or roles, select the users and roles, and then selectApply.
 TIP: appears next to a user or role that is already assigned to a group. You can assign the group to a user or role from Project viewby dragging the group to the user or role inProject view. appears next to a user or role that is already assigned to a group. You can assign the group to a user or role from Project viewby dragging the group to the user or role inProject view.
The group appears assigned to the user or role on the dashboard page. 
Provide Feedback