View alarms in standard time zone
    To view alarms in the standard time zone, you can display alarms events in the 
Alarm Grid
 and Alarm History Grid
 in the standard UTC time zone. Configure the time zone for the grid object in Template Libraries
.- Select.Template Libraries
- InTemplate Libraries, selectWidgets.
- DragAlarm gridorAlarm history gridfromWidgetsto the desired node in theUIfolder.
- InTemplate Libraries, selectClose.
- InProject view, expand the alarm grid and selectAlarmsDataGrid.
- inProperties, expandTimestamp.
- In theTextproperty, right-clickComplex Dynamic Linkand then selectReset value.
- Select. Change Dynamic Link Change Dynamic Link
- In the Dynamic Links window, configure either:- Alarm Grid. ExpandAliases, select , and then select theTimevariable.
- Alarm History Grid. ExpandAliases, select , and then selectLocalTime. AfterLocalTime, selectand then type Time. Time.
 
- ChooseSelect.
standard time zone
    
Provide Feedback