Time zones for alarm events
    At runtime, the 
Data grid
 object of the Alarm grid
 and Alarm log grid
 objects display the local time of events in the Timestamp
 column: | Object | Timestamp | 
|---|---|
| Alarm grid | Set a dynamic link in the  Timeproperty. | 
| Alarm history grid | Set a dynamic link in the  Timeproperty with a node pointer. | 
In projects that support remote sessions, devices with different local time settings can display different time zones in the widgets. The timestamp of the widget displays in the local time zone of the device, even when events occur in different time zones. In the 
Timestamp 
column of the Alarm grid
 or Alarm history grid
, set a converter of type Expression evaluator
 with the sum of the properties {Item}Time
 and {Session}TimeZoneOffset
. See  View alarms in remote local time zone.Provide Feedback