Manage data uploaded from a device
    Retain or delete data from retentivity storage for a project that was uploaded from a device.
Prerequisites
- Upload a project from device. See Open a project.
- To manage data uploaded from a device
- InProject view, hover over a retentivity storage and select. 
- InApply retained data, select either:- Apply. Apply data retained from the project that was uploaded from the device.
- Delete. Discard data retained from the project that was uploaded from the device.
- Cancel. Cancel the operation.
 
data
upload
    
Provide Feedback