Duplicate a project
    Duplicate a project to use an existing project as a template for a new project.
- Open the project to be copied and then from the main menu, selectSave as.
- InSave project as, complete:- Name. The name of the new project.
- Location. The storage location of the project files. The duplicated project is stored in the same location as the original project by default. Select the folder icon to browse to a new location.
- (optional)Use Version Control. Select to save your project in a Git repository.TIP: In order to use version control, FactoryTalk Optix project names and repository names must match. The project and repository names must contain only alpha numeric characters, numerals, periods, dashes, and underscores.
 
- SelectOK.
duplicate
template
    
Provide Feedback