Variables
    A variable is an attribute of an object. Assign a value to a variable to display the value at runtime.
View variables from either:
      
- Project view. Navigate to the folder containing the variables. TheUIfolder cannot contain variables.
- Properties. Select an object, type, or variable inProject viewor select and object in the editor. The variables or properties for the selected item appear inProperties.
attribute
value
    
Provide Feedback